The CardInfo sketch works fine.
I am trying to write a simple text file to the SD card.
I am getting error message Error opening Data.txt which means the SD.open( ) failed.
Data.txt does not exist but according to the documentation the file should be created.
I am not sure what I am doing wrong as this sketch is based on an example sketch for the SD library.
#include <SD.h>
#include <SPI.h>
const int chipSelect = 4;
Sd2Card card;
void setup()
{
Serial.begin(9600);
//pinMode(10, OUTPUT);
while (!Serial)
{
; // wait for serial port to connect. Needed for native USB port only
}
if (!card.init(SPI_HALF_SPEED, chipSelect))
{
Serial.println("Initialization failed.");
return;
}
else
{
Serial.println("Initialization passed.");
}
}
void loop()
{
File myFile = SD.open("Data.txt", FILE_WRITE);
if (myFile)
{
for (int i = 0; i < 101; i++)
{
myFile.print(i);
myFile.print(" multiplied by two is ");
myFile.println(i * 2, DEC);
}
Serial.println("Finished");
myFile.close();
}
else
{
Serial.println("Error opening Data.txt");
}
//do nothing else
do
{
}
while(1);
}