Hi! I am trying to get a PIC microcontroller to talk to the bluetooth bee, but I want feedback about the commands I send to it. I have the bee connected to the UartSBee module, and this is connected to my PC with a USB cable. They chat using the SSCOM terminal program. I also have the RX UART port of my microcontroller connected to the TX UART port of the UartSBee.

I can see status messages on the SSCOM terminal, confirming the commands I send.
Example: I send “+STWMOD=1”, I get:
OK
WORK:MASTER
+BTSTATE:0
+BTSTATE:1
Problem: How do I get these messages sent to the Rx UART port of my microcontroller? I have tried connecting the Rx port of my uCtrl to the Tx of the Bluetooth bee, but I just get the same command echoed back, and no confirmation messages.
Example: I send “+STWMOD=1” through the SSCOM to the bee
I get:
+STWMOD=1
from the Rx port of my uCtrl, even though I can see the
OK
WORK:MASTER
message on SSCOM. How do I get the status and confirmation messages to arrive to my uCtrl? I want it to say “OK / WORK: MASTER / etc.”, too.

Thank you!