Hello !!
i have made a medium project using Wifi on WIOT.
i have a problem when the wifi connexion is lost, all my tasks seems to hang…
after some investiguation, i can see something wrong when calling udp.begin(xx) when the Wifi is being lost.
here my code (slightly modified example to query NTP server)
static time_t _getNTPtime(void)
{
// module returns a unsigned long time valus as secs since Jan 1, 1970
// unix time or 0 if a problem encounted
WiFiUDP udp;
unsigned long epoch=0;
const int NTP_PACKET_SIZE = 48; // NTP time stamp is in the first 48 bytes of the message
byte packetBuffer[NTP_PACKET_SIZE]; //buffer to hold incoming and outgoing packets
//initializes the UDP state
//This initializes the transfer buffer
Serial.println("Sync time with NTP");
udp.begin(WiFi.localIP(), 2390);
_sendNTPpacket(&udp, timeServer, packetBuffer, NTP_PACKET_SIZE); // send an NTP packet to a time server
// wait to see if a reply is available
delay(1000);
if (udp.parsePacket())
{
Serial.println("udp packet received");
// We've received a packet, read the data from it
if (udp.read(packetBuffer, NTP_PACKET_SIZE)==NTP_PACKET_SIZE) // read the packet into the buffer
{
//the timestamp starts at byte 40 of the received packet and is four bytes,
// or two words, long. First, extract the two words:
unsigned long highWord = word(packetBuffer[40], packetBuffer[41]);
unsigned long lowWord = word(packetBuffer[42], packetBuffer[43]);
// combine the four bytes (two words) into a long integer
// this is NTP time (seconds since Jan 1 1900):
unsigned long secsSince1900 = highWord << 16 | lowWord;
// Unix time starts on Jan 1 1970. In seconds, that's 2208988800:
const unsigned long seventyYears = 2208988800UL;
// subtract seventy years:
epoch = secsSince1900 - seventyYears;
}
else
{
Serial.println("udp packet not complete");
}
}
// not calling ntp time frequently, stop releases resources
udp.stop();
return epoch ;
}
i have enabled the verbose mode for RPCWiFi and added some more trace inside udp.begin fonction…
Sync time with NTP
[E][WiFiUdp.cpp:42] begin(): before stop
[E][WiFiUdp.cpp:44] begin(): after stop
[D][WiFiGeneric.cpp:383] _eventCallback(): Event: 5 - STA_DISCONNECTED
[W][WiFiGeneric.cpp:407] _eventCallback(): Reason: 0 - MAX
Disconnected from WIFI access point
WiFi lost connection. Reason: 0
As you could see, the wifi disconnected event is rised after i begin to deal with udp.
and the task trying to call udp.begin is blocked after the 1st instruction (stop()![]()
The instruction that is probably waiting infinitly something seems to be "socket’
uint8_t WiFiUDP::begin(IPAddress address, uint16_t port){
log_e("before stop");
stop();
log_e("after stop");
server_port = port;
tx_buffer = new char[1460];
if(!tx_buffer){
log_e("could not create tx buffer: %d", errno);
return 0;
}
if ((udp_server=socket(AF_INET, SOCK_DGRAM, 0)) == -1){
log_e("could not create socket: %d", errno);
return 0;
}
log_e("after socket");
int yes = 1;
if (setsockopt(udp_server,SOL_SOCKET,SO_REUSEADDR,&yes,sizeof(yes)) < 0) {
log_e("could not set socket option: %d", errno);
stop();
return 0;
}
log_e("after setsockopt");
struct sockaddr_in addr;
memset((char *) &addr, 0, sizeof(addr));
addr.sin_family = AF_INET;
addr.sin_port = htons(server_port);
addr.sin_addr.s_addr = (in_addr_t)address;
if(bind(udp_server , (struct sockaddr*)&addr, sizeof(addr)) == -1){
log_e("could not bind socket: %d", errno);
stop();
return 0;
}
log_e("after bind");
fcntl(udp_server, F_SETFL, O_NONBLOCK);
return 1;
}
it seems WiFi.status() can also be blocking… in this case
hereunder, 1 task use HTTPClient for a request on a server… (and never returns)
1 other task try to start a NTP sync…but WiFi.status() never returns also…
all tasks using rpcWifi are now blocked infinitly…
Read measurements
[V][HTTPClient.cpp:236] beginInternal(): url: http://someip/somerequest.php
[D][HTTPClient.cpp:277] beginInternal(): host: someip port: 80 url: /somerequest.php
[D][HTTPClient.cpp:563] sendRequest(): request type: ‘POST’ redirCount: 0
[D][WiFiGeneric.cpp:383] _eventCallback(): Event: 5 - STA_DISCONNECTED
[W][WiFiGeneric.cpp:407] _eventCallback(): Reason: 0 - MAX
Disconnected from WIFI access point
WiFi lost connection. Reason: 0
Sync time from NTP
the associated code:
Serial.println("Sync time from NTP");
if (WiFi.status() == WL_CONNECTED)
{
time_t ntpdt=_getNTPtime();
the _getNTPtime() function is the one at the begining of this post…
It seems there is a kind of deadlock situation somewhere in rpcWifi…
is someone can help ??
oh, i forgot, i’m using FreeRTOS and plateform.io, memory & stack seems to be good enough…
Eric.