routing line antenna u.fl lora e5

Hi!,
I are working in developing a system for monitoring and control of critical variables on greenhouse iot based. we are desing the pcb with wio-e5 like module loraWAN and ESP32 like MCU for our node. I need help for routing the line connector U.FL for the antenna 915Mhz.
In the datasheet I did not see any consideration about this. but in the other side I did read about considering 50 ohm for the route. how can I actually do this? is necessary?, Also, I hace seen some schematics that dont use 0 ohm resistors and bypass capacitors. but the lora E5 datasheet does show them. ¿can someone out there help me?