Hi
I was just wondering if it’s possible to create a round PCB (approx 85mm dia) with a 40 mm dia hole in the middle (essentially a ring shaped PCB) with the fusion service?
Many thanks
Hi
I was just wondering if it’s possible to create a round PCB (approx 85mm dia) with a 40 mm dia hole in the middle (essentially a ring shaped PCB) with the fusion service?
Many thanks
Hello,
It should be OK. But you should send your gerber file to us first because we need to confirm if it’s really possible.
Regards,
Simon
Thanks - I’ve not done any of the layout yet - I didn’t want to start before I new it was possible
I’ll send something along in due course…
I’ve not progressed this any further due to other commitments - it’s probably worth you submitting your design and seeing what they say
Ant
Round PCB outline is fine. Seeed will route the edges to basically any shape you wish. The board size is simply the smallest square it will fit in, so a 4.8cm diameter circle is fine for the 5x5cm service.
The original poster was asking about internal routing to cut out a smaller circle from the middle also.