Round Display with Xiao C3, C6, S3 & S3-Plus Test Examples

Hi there,

So I have been asked to provide some working demo’s for the Seeed Round Touch display. It works with All the Xiao’s that have enough ram. Today we have the C6 and , S3-Plus. Seen here. Link to C3 is Here

Both units are setup the same, SD cards are formatted FAT32 and contain a /gif folder with two gifs, wink-monkey.gif , pjglasso.gif. These demo loops contain the Animated gif code example also merged in.

I have included the BIN files, if you would like to flash it to test your devices function. Feel free to ask any questions and I’ll provide answers when possible and the code involved. Do read the Wiki for the ROUND Display to gain a basic understanding of how and why it works. A Lot of people struggle to get it working, because they don’t follow the directions. :face_with_hand_over_mouth:
The serial port output is the value on the display , BTW for the Touch Demo. :+1:

To test these BIN files with your hardware. Use the ESP Flash Tool
copy the BIN file to the same DIR as the Tool. Open the tool and Set the address to 0x00 and select the bin you want. (…) turn on the check mark and the click start You can tell if it worked.:+1: If your not familiar with this tool, you should be. Info Here on it.

Touch_Ring_Meter_Demo_C6.zip (196.1 KB)
AI_ROUND_DEMO_C6.zip (219.7 KB)

Load the tool , check the Chip info, Select the BIN file, Base address (0x00) set the Comm Port, Flash Mode, click START. Bob’s your Uncle…and You can tell when it’s done.

YOU MUST MANUALLY Press the Xiao RESET button.

:grin:
If you have problems It’s usually between the Keyboard and the Floor So… Enjoy the Video :+1:

AL_ROUND_DEMO_S3_plus.zip (258.5 KB)
Touch_Ring_Meter_Demo_S3-Plus.zip (230.9 KB)

The Next will be some BLE slaved controls… Stay tuned! :v:

GL :slight_smile: PJ :crossed_fingers:

Hi PJ,

You are the legend! Appreciated for the projects you shared!

Regards,
John

Hi there,

So I’m just getting Started :grin:

Here is the TouchRing Video Demo and code for you to compile yourself.

The TouchRing Meter Demo showcases an elegant and responsive user interface on the Seeed Studio 1.28" Round Display powered by the GC9A01 driver. Featuring a 240×240 pixel TFT panel and capacitive touch input via the CST816S controller (I2C).

This code project creates an interactive analog-style ring meter that responds to Touch and up/down swipe gestures. The visual interface includes a color-coded arc scale (green to red), a central numeric value display, and on-screen ‘+’ and ‘–’ indicators.

The demo unit is powered by the Seeed Studio Xiao ESP32-C6 or S3 and uses the TFT_eSPI and lv_xiao_round_screen libraries for high-performance graphics and touch handling.
Users can drag their finger to adjust a value between 0 and 99, with immediate visual feedback. The layout is optimized for the round form factor, making it an ideal base for control knobs, gauges, or user input widgets. This standalone version is clean, smooth, and PHAT—perfect for embedded UI prototypes or hardware demos.

AMA
HTH
GL :slight_smile: PJ :v:

// ===================================================================================
// PJ DEMO FINAL - Xiao ESP32C6 & ESP32S3-Plus & Round Display
// Rev        : v1.3
// Build Time : __DATE__ and __TIME__
// Features   :Touch Test Ring meter DEMO 1.4 
// Authors  : Pj Glasso, & Embedded AI Assistant 
// ===================================================================================

#include <TFT_eSPI.h>
#include <SPI.h>
#define USE_TFT_ESPI_LIBRARY
#include "lv_xiao_round_screen.h"  // CST816S touch driver

#define RADIUS 120
#define SEEED_GREEN 0x07E0
#define SEEED_BLUE  0x001F
#define YELLOW      0xFFE0
#define ORANGE      0xFD20
#define RED         0xF800
#define GREY        0x2108
#define WHITE       0xFFFF
#define BLACK       0x0000

int currentValue = 50;
lv_coord_t touchX, touchY;

// -----------------------------------------------------------------------------------
void setup() {
  Serial.begin(115200);
  delay(500);
  Serial.println("=== Touch Ring Meter Demo v1.4 Start ===");
 
  pinMode(TOUCH_INT, INPUT_PULLUP);
  Wire.begin(); // SDA=D4, SCL=D5

  tft.begin();
  tft.setRotation(0);
  tft.fillScreen(BLACK);
  tft.setTextDatum(MC_DATUM);
  tft.setTextColor(WHITE, BLACK);
  showMainScreen();
    delay(500);
    tft.fillScreen(TFT_BLACK);

  drawPlusMinus();
  ringMeter(currentValue, 0, 99, 0, 0, RADIUS);
  drawText(String(currentValue), 120, 125, currentValue);
}

// -----------------------------------------------------------------------------------
void loop() {
  static int lastValue = -1;

  if (chsc6x_is_pressed()) {
    chsc6x_get_xy(&touchX, &touchY);

    int dx = touchX - 120;
    int dy = touchY - 120;

    float dist = sqrt(dx * dx + dy * dy);

    if (dist > 20) {  // Ignore center tap
      if (abs(dy) > abs(dx)) {
        if (dy < -10 && currentValue < 99) currentValue++;
        if (dy > 10 && currentValue > 0) currentValue--;
      }
    }

    if (currentValue != lastValue) {
      ringMeter(currentValue, 0, 99, 0, 0, RADIUS);
      drawText(String(currentValue), 120, 125, currentValue);
      lastValue = currentValue;

      //Serial.printf("Touch (X:%d Y:%d) Value: %d\n", touchX, touchY, currentValue);
      Serial.printf("%d\n", currentValue);

    }
  }

  delay(30);
}

// -----------------------------------------------------------------------------------
int ringMeter(int value, int vmin, int vmax, int x, int y, int r) {
  x += r;
  y += r;
  int w = r / 3;
  int angle = 150;
  int v = map(value, vmin, vmax, -angle, angle);
  byte seg = 3;
  byte inc = 6;

  for (int i = -angle + inc / 2; i < angle - inc / 2; i += inc) {
    float sx = cos((i - 90) * DEG_TO_RAD);
    float sy = sin((i - 90) * DEG_TO_RAD);
    uint16_t x0 = sx * (r - w) + x;
    uint16_t y0 = sy * (r - w) + y;
    uint16_t x1 = sx * r + x;
    uint16_t y1 = sy * r + y;

    float sx2 = cos((i + seg - 90) * DEG_TO_RAD);
    float sy2 = sin((i + seg - 90) * DEG_TO_RAD);
    int x2 = sx2 * (r - w) + x;
    int y2 = sy2 * (r - w) + y;
    int x3 = sx2 * r + x;
    int y3 = sy2 * r + y;

    uint16_t color = GREY;
    if (i < v) {
      int mapped = map(i, -angle, angle, 0, 99);
      if (mapped <= 24) color = SEEED_GREEN;
      else if (mapped <= 50) color = SEEED_BLUE;
      else if (mapped <= 75) color = YELLOW;
      else if (mapped <= 86) color = ORANGE;
      else color = RED;
    }

    tft.fillTriangle(x0, y0, x1, y1, x2, y2, color);
    tft.fillTriangle(x1, y1, x2, y2, x3, y3, color);
  }

  return x + r;
}

// -----------------------------------------------------------------------------------
void showMainScreen() {
  String mcuType = "Unknown";

#if CONFIG_IDF_TARGET_ESP32C6
  mcuType = "ESP32-C6";
#elif CONFIG_IDF_TARGET_ESP32C3
  mcuType = "ESP32-C3";
#elif CONFIG_IDF_TARGET_ESP32S3
  mcuType = "ESP32-S3";
#elif CONFIG_IDF_TARGET_ESP32
  mcuType = "ESP32";
#endif

  // Optional: Detect S3-Plus specifically
#ifdef ARDUINO_XIAO_ESP32S3
  mcuType = "ESP32-S3-Plus";
#endif

  tft.fillScreen(TFT_BLACK);
  tft.setTextColor(SEEED_GREEN);
  tft.setTextSize(2);
  tft.setCursor(40, 40);
  tft.println("Seeed Studio");

  tft.setTextColor(0xFFFF);
  tft.setCursor(30, 90);
  tft.print("MCU: ");
  tft.println(mcuType);

  tft.setCursor(30, 135);
  tft.println("Rev: PJ Demo v1.3");

  delay(3000);
}


void drawText(String text, int x, int y, int value) {
  uint16_t color = (value > 86) ? RED : WHITE;
  tft.setTextColor(color, BLACK);
  tft.setTextDatum(MC_DATUM);
  tft.setTextSize(3);
  tft.drawString(text, x, y);
}

// -----------------------------------------------------------------------------------
void drawPlusMinus() {
  tft.setTextDatum(MC_DATUM);
  tft.setTextSize(3);
  tft.setTextColor(WHITE, BLACK);
  tft.drawString("+", 120, 30);   // Top center
  tft.drawString("-", 120, 210);  // Bottom center
}

Link to it in the BLE…
🧐 Round Display w/TouchRing BLE Xiao C6 & S3-Plus

Wow I am totally going to try to implement this!

Hi there,

It’s good hardware and works well with the right LIB’s the Gesture stuff works well with it too, but I find the S3 definitely makes it perform. It works with most of the Xiao’s but the Nrf and other ESP’s are slower and a tad less responsive and crisp compared to what you get with a S3 in the seat! :+1:

Would be cool to fit it to the S3&WIo-SX1262 and get that going with the mesh :grin:

HTH
GL :slight_smile: PJ :v:

The S3 is definatelly the best pairing for it.

The nrf’s : not soo much. Mostly a seeed issue, keeping up the backend. like conflicts between tft-espi and bluetooth, forcing you to use arduinogfx.

It will work, but is a lot more hassle. Even thoug the nrfs (at least the one I tried) are considerably faster.

Seeed itself aso advices the S3 above the nrfs.

The gesture stuff works, but it’s not refined anough yet. Like I have a touch circle and a gesture to go to the next streen. Sometimes it thinks the usage of the touch cicle is a gesture.

Useful info , thank you!

Has anyone connected other components to the esp32-c3, being installed on the round display? I need to connect to a R558S fingerprint sensor.

Hi there

And Welcome Here..

So, the Round with an S3 Plus gives You all you need. You can connect anything to it, check out my 6 Sensor Node demo, video, or the Breakdown video of how its connected to the B2B connector with more_I/O board attached,

best viewed Full screen :grin:

HTH
GL :slight_smile: PJ :v:

The Grow R558S is a round, ring-mount capacitive fingerprint module with an integrated RGB ring indicator light. Internally, it uses the Synochip/Grow protocol compatible with standard R502 / R503 / AS608 command sets over TTL UART.

Hardware Pinout & Wiring

The R558S uses a 6-pin 1.0mm pitch harness (colors are typical for Grow modules; check your cable labeling):

  • Pin 1 (Red): VCC (3.3V power)

  • Pin 2 (Yellow): TXD $\rightarrow$ Connects to MCU RX (3.3V TTL)

  • Pin 3 (White): RXD $\rightarrow$ Connects to MCU TX (3.3V TTL)

  • Pin 4 (Black): GND (Ground)

  • Pin 5 (Blue): WAKEUP / TOUCH_OUT (Active HIGH pulse when finger touches sensor; tie to an ESP32 wake pin to keep the MCU in deep sleep until touched)

  • Pin 6 (Green): 3.3V_TOUCH (Powers the capacitive touch detection circuit; typically tied together with Pin 1 VCC)

You need to enroll the print first , FYI…
Here is a test code, you can try.

#include <Adafruit_Fingerprint.h>

// Set to your hardware serial pins
#define SENSOR_RX_PIN 44  // Connects to R558S Yellow (TX)
#define SENSOR_TX_PIN 43  // Connects to R558S White (RX)

HardwareSerial mySerial(1);
Adafruit_Fingerprint finger = Adafruit_Fingerprint(&mySerial);

void setup() {
  Serial.begin(115200);
  while (!Serial) delay(10);
  Serial.println("\n--- Grow R558S Test ---");

  // R558S default UART: 57600 baud, 8N1
  mySerial.begin(57600, SERIAL_8N1, SENSOR_RX_PIN, SENSOR_TX_PIN);
  finger.begin(57600);
  delay(150);

  if (finger.verifyPassword()) {
    Serial.println("Found R558S sensor!");
  } else {
    Serial.println("Sensor not found. Check power, swapped RX/TX, or baud rate.");
    while (1) { delay(10); }
  }

  finger.getParameters();
  Serial.print("Sensor capacity: "); Serial.println(finger.capacity);
  Serial.print("Device address: 0x"); Serial.println(finger.device_addr, HEX);
}

void loop() {
  uint8_t p = finger.getImage();
  if (p == FINGERPRINT_NOFINGER) {
    delay(50);
    return;
  }

  if (p == FINGERPRINT_OK) {
    Serial.println("Finger detected!");
    p = finger.image2Tz();
    if (p == FINGERPRINT_OK) {
      p = finger.fingerSearch();
      if (p == FINGERPRINT_OK) {
        Serial.print("Match found! ID #"); Serial.print(finger.fingerID);
        Serial.print(" (Confidence: "); Serial.print(finger.confidence); Serial.println(")");
      } else {
        Serial.println("No match in database.");
      }
    }
  }
  delay(500);
}

Controlling the RGB Ring LED

// Modes: 1 = Breathing, 2 = Flashing, 3 = Always ON, 4 = Always OFF
// Colors: 1 = Red, 2 = Blue, 3 = Purple (Combine red+blue)
// Speed: 0x00 to 0xFF; Count: 0 = infinite, 1-255 = cycle count

// Example: Flash Blue 2 times quickly (successful match)
finger.LEDcontrol(FINGERPRINT_LED_FLASHING, 25, FINGERPRINT_LED_BLUE, 2);

// Example: Solid Red for 1 second (access denied)
finger.LEDcontrol(FINGERPRINT_LED_ON, 0, FINGERPRINT_LED_RED, 0);

The R558S ring light can be driven using the LEDcontrol command provided in the Adafruit library:
:wink: GL :v:

Yes, I have connected a MMWave sensor (256kBaud) to the second serial port of the XIAO ESP32-C3. I had to disable the TP_INT (same GPIO as RXD). I then just “polled” the touch screen.

Worked fine BUT the 'C3 doesn’t really work “well” with a Seeed Round Display if complicated “screens” are being used (eg menus, multiple pages, fast updates pages etc).

Yep, that matches what I’ve seen too. The C3 can drive the Round Display, but once the UI gets a bit richer it starts to feel tight — especially with frequent redraws, touch handling, and another UART device in the mix.

Polling touch after disabling TP_INT is a perfectly reasonable workaround on the C3, as long as the UI doesn’t need super responsive gestures. For anything menu-heavy or with live sensor pages, I’d usually steer people toward the S3 / S3 Plus instead. The extra headroom makes the Round Display experience much smoother and leaves more GPIO/UART flexibility for sensors.

Round Display does …

Dragon Detector

A firmware developed by Valleytech Custom Solutions.

The source repository, build pipelines, and web installer tools are hosted under the Valleytech GitHub

It is an open-source tool built for ESP32 hardware profiles (such as the XIAO and round display combinations) that performs passive Wi-Fi and Bluetooth Low Energy (BLE) scanning, RSSI signal tracking, and target mapping rendered in the iconic Dragon Ball radar interface.

We are seeing more and more of these kinds of devices using Xiao also, like the FLOCK camera tracker , detector.. by Kernel Panic , I think ? The Size and power of Xiao is evident.

  1. OUI Spy / Flock-You
  2. SignalSweep
  3. ESP32 Marauder
  4. Biscuit / Biscuit Ultra
  5. Rayhunter (Cell-Site / IMSI Catcher Detection)

Round display is IT! for a cool factor , Choose your MCU
They all Work , albeit some better than one :grin: (c3) :+1:

I want to see a 4" round display in Seeeds catalog, That would be Great and and E-paper would be knock out of the PARK boi! :smile:

As You were
:saluting_face:

GL :slight_smile: PJ :v: