This did work for the ESP32S3, I used the following libraries:
FQBN: esp32:esp32:XIAO_ESP32S3
Using board ‘XIAO_ESP32S3’ from platform in folder: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8
Using core ‘esp32’ from platform in folder: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8
Multiple libraries were found for “SD.h”
Used: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8\libraries\SD
Not used: D:\Documents\Arduino\libraries\SD
Multiple libraries were found for “lv_xiao_round_screen.h”
Used: D:\Documents\Arduino\libraries\Seeed_Arduino_Round_display
Not used: D:\Documents\Arduino\libraries\HardwareTest
Using library SPI at version 2.0.0 in folder: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8\libraries\SPI
Using library SD at version 2.0.0 in folder: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8\libraries\SD
Using library FS at version 2.0.0 in folder: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8\libraries\FS
Using library Seeed Arduino Round display at version 1.0.0 in folder: D:\Documents\Arduino\libraries\Seeed_Arduino_Round_display
Using library lvgl at version 8.3.4 in folder: D:\Documents\Arduino\libraries\lvgl
Using library Wire at version 2.0.0 in folder: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8\libraries\Wire
Using library TFT_eSPI at version 2.5.43 in folder: D:\Documents\Arduino\libraries\TFT_eSPI
Using library SPIFFS at version 2.0.0 in folder: C:\Users\arduinoUser\AppData\Local\Arduino15\packages\esp32\hardware\esp32\2.0.8\libraries\SPIFFS
I’ve seen other were able to use esp board driver v2.11 and some with higher versions of the LVGL library. Also, it appears some have had success with arduino_Graphix library and selecting display chip driver GC9A01.
Anyone had any luck with these other options?