Is it possible to publish a RGB LED Ring (24-WS2813 Mini) 3D or 2D DWG/DXF file. I need it for a CAD software.
Hi there~
Sorry to tell you that we actually don’t have any 3D or 2D DWG/DXF file.
But the inner diameter is 53.30mm and the outer diameter is 70.30 mm.
Thanks cheers
JL from Seeed.
Thanks. Can you please reply the inner and outer diameter of RGB LED Rings (20 and 24).
Hi
RGB LED Ring(20): inner diameter 43.00 mm and outer diameter 60.00 mm.
RGB LED Ring(24): inner diameter 53.30 mm and outer diameter 70.30 mm.
Thanks