RFBee firmware updating

@icing
I was reading the datasheet, and I noticed it claimed 2 analog inputs. This is confusing me because, 1 10 input, adc7 is mapped, but adc6 the other does not appear to be brought out. Now from reading the 168 datasheet 6 of the PortC pins can be made analog inputs, 8 bits, but that doesn’t add up to 2. Can you clarify what is meant here? I am simply curious as Hans has things working well enough I am getting read to try so configurations with sensors and the like.

Also since somebody asked I was thinking of connecting the i2c interface in a slave config. the pins are mapped so it should fly, but I thought I would double check.