RFBee firmware updating

Great work. I gave it a little thought and this is what I came up with as feedback. Again have a great vacation.

Frankly I think WOR should be a sleep argument to the SL command not a mode, as the previous mode should be unchanged. This is the issue I have with the current low power, it really isn’t a mode like the others. Is Low Power really a mode, or simply better controlling of the radio subsystem. In WOR Low Power I do not see that the users should notice any change in behavior.
(Is this correct? If it is I will argue for it being the normal state.)

I view it as there are several general states here.
Reduce Power until event occurs, where event is anyone of
WOR
Interrupt received.
Serial received.
To me this is not a mode, but a efficiently wait state.

    Hibernate, ignoring Local events, other than watch dog if independently enabled.
            WOR
            WatchDogTimer  if independently enabled.
            External circuit trigger.
                    This is sleep on radio, node is a remotely controlled slave.

     Sleep.
            Radio traffic ignored.
            WatchDogTimer  if independently enabled, or other external wakeup
            Serial data ignored.
                     Shutdown for until locally kicked or watchdog.

There is one more option to complete things, but its value is not as clear to my fuzzy thinking.
Turn off radio, but leave the 168 going. That is this is
SleepRadio, but save state.
168 is uneffected. Radio is pwr’ed down until wake. This is the best candidate for a MD to me. This is really Mode radio power downed, and until an ATMD is issued to wake it up and set the resumed state it is powered down.

Is there a need for IDLE radio, not sleep, not WOR, but just stay in the IDLE state? This condition is implied by transmit mode, where the radio goes to this state when there is no data to send, but does this state as a mode need to exist? This is leave the radio up and calibrated, but not doing anything. It is clear that this state is used, and may speed the transition to other states. I am just not clear if the speed up it offers is enough to expose it in the model.