RFBee firmware updating

Hi Team,

Thank you so much for the updating.

Hans, you are right, CRC OK does not mean packet is fly passed to the FIFO, which causes the problem we met. The setting of GO0 to 0x01 can solve this problem.
However, I still found several problems:

  1. When in ATCF1~3, RFBee doesn’t work well, as the receiver can receive only one byte what ever the transmitter sends.

  2. In ATCF0(default configuration), the RFBee will receive some nonsense bytes when keep it silent there. I think it is the interruption of the RF signal around it. And when we set GDO0 with 0x01, which also means it has no CRC, the interruptive RF data may be received by the RFBee.

How about your testing result?

Regards,

-Icing