Hi,
Can anyone help to get the following done:
- have some code for an Arduino + Wireless Proto Shield + RF Bee functioning as a wireless sensor base station;
- have some code for the standalone node (Firmware 1.1 works) to send to the base station.
I have no clue how to use the RFBee with the Wireless Proto Shield and Arduino UNO to receive data from standalone nodes. There is no code on any forum on the net that does this and I have no clue which firmware to use on the base station (Arduino etc.). The standalone one can be figured out, it can run either RF Bee master or slave code.
Seeedstudio has not provided any sample for this combination.
Cheers and thanks in advance!