- I can ping out from reTerminal and ping my reTerminal but every time I try smb or “network” to access a network NAS drive I keep getting the error “specified location is not supported”
You mean you are trying to access a NAS drive using the reTerminal? Are you connected via Ethernet or WiFI? Also, how are you accessing the NAS drive? Can you tell me the steps? I can reproduce on my end with my NAS and reTerminal.
Currently, I am using Ethernet. In a reTerminal TERMINAL window I can ping my NAS drive on my local network (192.168.1.xx). From my Windows 10 computer I can ping my reTerminal. I am connected to my NAS network drive all the time on my Windows PC. I also have a RP400 system running Buster from which I can access my NAS network drives using the File Manager and Networks. I can also gain access to the Internet
Steps attempted to access my local Network:
reTerminal “out of the box” going through Getting Started with reTerminal - Seeed Wiki (seeedstudio.com) Steps 1 – 10 but SKIPPING the update and upgrade!
Enabled: ssh, serial port, serial console (everything except VNC so far)
Then rebooted.
Checked Network and both eth0 and wlan0 are active.
Clicked on “Chromium” icon and navigated to several websites with no problem.
File Manager:
Click “Go”
Click “Network”
Result: “Error” “The specified location is not supported”
Type: Network://
Result: Nothing
Type: smb://
Result: “Error” “The specified location is not supported”
Tried to use “ssh” to login to reTerminal
Had to use ip address instead of pi@reTerminal…
Used the password I changed to and the default password and received:
Permission denied (publickey,password).
Never asked for username
I also have a RP 400 running Buster as well
When I click on File Manager “GO” and Network, I can see my desired NAS device. I can then Login to it. I did not Install any additional network related tools or programs.