The reTerminal’s heatsink is covered by the E10-1 Expansion Board. This can cause the temperature of the reTerminal to increase as there is not enough exposed surface area for air flow over the heat sink.
Please consider one of the following:
- an optional taller heatsink if the E10-1 is connected.
- a rear case with a bigger heatsink extending to all sides of a reTerminal.
- A peltier module connected to the bigger heatsink in option (1).
Thank you.