I’m trying to find a PCIe wifi adapter that will work with the PCIe slot in the E10-1 expansion.
I’ve tried three different mini-PCIe cards, based on the MPE-AX3000H, 7265HMW, and Intel 7260.HMW chipsets but none of them even show up in lspci or dmesg.
I have the switch in the PCIE position.
Is there something else I need to do for the cards to be recognized? Is there a specific adapter that is known to work/supported?
For our reTerminal use case we need two wifi interfaces so I’m trying to add a second interface using the expansion.