Hi All - I’ve been working to get a reTerminal working again that has been laying around for a while not doing anything, so I decided to get it up and running again. I initially had it working and the display patched when I first got it but something happened and I lost the display. I started going through the procedure again from scratch using the same guide as last time (FAQs for reTerminal Usage | Seeed Studio Wiki) and all was going perfectly,
- Disabled reTerminal display in /boot/config, Verified STM32 > 1.7 using:
i2ctransfer -y 1 w2@0x45 0x9b 0x01
No issues so far…
-
Downloaded 2022-05-29-reTerminal-V1.9 [STM32G030F6_R2.bin] |
(Release 2022-05-29-reTerminal-V1.9 · Seeed-Studio/seeed-linux-dtoverlays · GitHub) -
The 1.9 firmware package did not include a STM32Flash utility, so I grabbed STM32Flash from V1.8 listed below
-
Pushed files to device, made STM32Flash executable
-
Fat fingered the command to make STM32 bootable…

i2ctransfer -y 1 w2@0x45 -0x9b 0x01
Error: Invalid data byte
Error: faulty argument is '-0x9b'
Soooo, now even the corrected command consistently returns
i2ctransfer -y 1 w2@0x45 0x9b 0x01
Error: Sending messages failed: Remote I/O error
Rebooted and the system starts fine and seems to operate without issue but its got the same issue when running the command.
Ill admit, I’m a bit new to anything i2c related. Will I need to reflash STM32 firmware some other way? Is it now permaborked? Any advice would be helpful on this <3