reTerminal bullseye pi camera

I recently flashed reTerminal with latest Raspberry OS (64-bit).
Here is the system info:
Linux reterminal 5.15.61-v8+ #1579 SMP PREEMPT Fri Aug 26 11:16:44 BST 2022 aarch64 GNU/Linux
And I cannot get pi camera working properly. sudo vcgencmd get_camera returns supported=0 detected=0, libcamera interfaces=0. The same camera works properly before reos.

I was wondering if this is a hardware issue or a software issue.

Thank you!

Hi @bh4cyi, the solution is relatively simple; I describe it below. In the config.txt file where the camera autodetection is, you change the one to a zero. Then you use the command dtoverlay + the reference of your camera and the parameter cam0. According to the link, this parameter adopts the default configuration for CAM0 in a Compute Module (CSI0, i2c_vc, and cam0_reg).

My OS Release:

PRETTY_NAME="Raspbian GNU/Linux 11 (bullseye)"
NAME="Raspbian GNU/Linux"
VERSION_ID="11"
VERSION="11 (bullseye)"
VERSION_CODENAME=bullseye
ID=raspbian
ID_LIKE=debian
HOME_URL="http://www.raspbian.org/"
SUPPORT_URL="http://www.raspbian.org/RaspbianForums"
BUG_REPORT_URL="http://www.raspbian.org/RaspbianBugs"

This is what my config.txt looks like, and that solved my problem.

#dtoverlay=ov5647,cam0
#dtoverlay=imx219,cam0
dtoverlay=imx477,cam0
#dtoverlay=adv7282m,cam0
camera_auto_detect=0

Regards

It works! Thank you very much! :metal: