Reterminal and libcamera

Hello,
I am trying to get reterminal working with a raspberry pi hq camera and libcamera commands.
I am using the 32 bit version of reterminal.
I have downloaded the libcamera, libepoxy, and libcamera-apps from github.
I have added dtoverlay=imx477 to the config.txt file.
Using vcgencmd get_camera returns with supported-2 detected-1
When i type libcamera-hello in a terminal window the return is ‘the system seems to be configured for the legacy camera stack’ .
Can anyone help determine what I am doing wrong?
Thank-you

Hi @KAYDE1 , the solution is relatively simple; I describe it below. In the config.txt file where the camera autodetection is, you change the one to a zero. Then you use the command dtoverlay + the reference of your camera and the parameter cam0. According to the link, this parameter adopts the default configuration for CAM0 in a Compute Module (CSI0, i2c_vc, and cam0_reg).

My OS Release:

PRETTY_NAME="Raspbian GNU/Linux 11 (bullseye)"
NAME="Raspbian GNU/Linux"
VERSION_ID="11"
VERSION="11 (bullseye)"
VERSION_CODENAME=bullseye
ID=raspbian
ID_LIKE=debian
HOME_URL="http://www.raspbian.org/"
SUPPORT_URL="http://www.raspbian.org/RaspbianForums"
BUG_REPORT_URL="http://www.raspbian.org/RaspbianBugs"

This is what my config.txt looks like, and that solved my problem.

#dtoverlay=ov5647,cam0
#dtoverlay=imx219,cam0
dtoverlay=imx477,cam0
#dtoverlay=adv7282m,cam0
camera_auto_detect=0

Regards

Hi jarain78,
Thanks for the response. It may take me some time but I will try this configuration.
kayde1