reTerminal and bullseye?

Hello @dq11,

You need to add the following line inside /boot/config.txt file:

dtoverlay=reTerminal,tp_rotate=1

Note: “dtoverlay=reTerminal” is already inside the above file by default. So you just need to add “,tp_rotate=1” after “dtoverlay=reTerminal”.

And then reboot. The touch will start to work as normal again.