Hi there,
Ok, no worries, we’ll figure it out.
Must have some corruption somewhere?
So if you press the reset button on the GV2 does it disconnect or reset while the port is connected if pressed ?
I may go load a Edge setup on one and try to get back to Senscraft. see if I can duplicate it. Either way a fresh Flash will be needed i’m sure.
The absence of the Info is a BIG red ARROW…
I assume you used the Xiao and Arduino to restore it? that method.
HTH
GL PJ
I saw the newest Tech from Nordic “nuclio” pretty wild stuff from them, and they are an Edge partner Edge needs work IMO. I’m glad there is competition in the space.
leaning towards program is ok , but bootloader must be nurfed?