Respeaker on raspberry Pi

Hi,

I have bought 2 ReSpeakers 4-Mic Array for Raspberry Pi and I’m trying to
set them up on a new Raspberry Pi B+ with a clean build of Raspian.

I am using this document for setting up:

http://wiki.seeedstudio.com/ReSpeaker_4_Mic_Array_for_Raspberry_Pi/#getting-started

At step 4 of install driver section when I run arecord -L I see:

pi@raspberrypi:~/seeed-voicecard $ arecord -L
null
Discard all samples (playback) or generate zero samples (capture)
default
playback
ac108

I have tried rebuild of raspbian and using 2 different Pis. Please help.

Thanks

Mat Walker

Hi

Mat,


1. Do you use Raspberry Pi 1 Model B+?

2. Which raspbian os do you use? We tested with latest raspbian OS Version: April 2019, Release date: 2019-04-08, Kernel version: 4.14, It works with my raspberry pi 3b/3b+.

3. We have build the image with drivers pre-installed. You can download and burn to SD card and see if it works.



4. Please let us know if you still have the issue with step3.

Thanks

best rgds
Bill

Hi Bill,



Thanks for your reply.



It’s a new Raspberry Pi 3 Model B +. I have two of them for a project with

Noobs SIM cards and I started with a clean install with latest OS:



Raspbian GNU/Linux 9 (stretch)

version 9 (stretch)



4.19.42-v7+ #1219 SMP Tue May 14 21:20:58 BST armv71 GNU/Linux



I found this on the forum yesterday with the same problem:



<URL url="https://forum7.seeedstudio.com/t/4-mic-linear-array-not-recognized/6678/2 text=“viewtopic.php?f=37&t=31995&p=53679&hili … 200#p53679”>https://forum7.seeedstudio.com/t/4-mic-linear-array-not-recognized/6678/2


Resinstalling the driver didn’t help but using your image solved the

problem. Your image takes me to an earlier core:



v4.14.52-v7+ #1123 SMP Wed Jun 27 17:35:49 SBST 2018 armv71 GNU/Linux



Next problem was that all the pip installs for DOA without keywords are

for Python 2. I resolved this by using pip3 and manually fixing Queue to

queue in mic_array.py.



Final problem was that the LED instructions are very confusing. The

vad_doa.py example in the Raspberry Pi instructions uses

pixel_ring.set_direction and this doesn’t work giving USB not found error.

Found this article

https://github.com/respeaker/mic_array/issues/18



So everything is working fine now.



Hope this helps. Maybe some of this information could go in the getting

started document.

HI Mat


Thanks for the feedback.

1. I will test Raspbian GNU/Linux 9 (stretch) version 9 (stretch) tomorrow.

4.19.42-v7+ #1219 SMP Tue May 14 21:20:58 BST armv71 GNU/Linux

2. "

DOA without keywords

", Current it is python 2.7. I will talk with software team and see their plan to move to python3


3. For the leds, please refer to https://github.com/respeaker/pixel_ring


Thanks

best rgds
Bill

HI Mat,


I talked with software team and they fixed the issue. So please run below commands as below.

sudo ./uninstall.sh
sudo reboot
sudo ./install.sh
sudo reboot


pi@raspberrypi:~ $ uname -a
Linux raspberrypi 4.19.42-v7+ #1219 SMP Tue May 14 21:20:58 BST 2019 armv7l GNU/Linux
pi@raspberrypi:~ $ arecord -l
**** List of CAPTURE Hardware Devices ****
card 1: seeed4micvoicec [seeed-4mic-voicecard], device 0: bcm2835-i2s-ac10x-codec0 ac10x-codec.1-003b-0 []
Subdevices: 1/1
Subdevice #0: subdevice #0
pi@raspberrypi:~ $


Thanks

best rgds
Bill

Hi Bill,



Thanks for sorting out the driver. I’ll try this next week once my event

is over. I have a stable, working system using your image.