Respeaker on Raspberry Pi 5

I am experiencing confusion about choosing a respeaker module for raspberry pi 5. I want to try the 2 Mic respeaker but from the description it only supports up to raspberry pi 4. is there a solution to determine the respeaker module that I can use on raspberry pi 5.

Please help

I have a problem with the two things I am trying to get it to work on. 1. Pi5 2. Pi zero 2 w. It seems the is an issue with mounting the kernel header of both. Can anyone confirm whether there is an update or a version which works?

I got the same problem, just bought the Raspberry Pi 5 and tried everything to make the driver work. It is unfortunately incompatible (see https://www.reddit.com/r/raspberry_pi/comments/1gdpvjl/help_with_driver_for_respeaker_2mics_pi_hat/). Does anyone know if there is support for this planned in the near future?