Hi,
I’d like to use my new MicArray v2 as a general usb mic device on mac, preprocessed for voice input.
Currently the factory firmware is installed. I see all 6 channels and input works, but the Audio MIDI Setup app cannot control specific channels on the device for me to prioritize channel 0 (processed for voice).
Alternatively I could change the firmware the 1-channel version but the forum recommends not to do this from a Mac - I’m not sure if this means not to update the firmware from a terminal window, which would be my approach.
Is there a way for me to select the correct channel on mac, or change the firmware?
Thanks
Hi there,
Yes, you can update the firmware to 1 channel firmware and you will get the processed audio.
You can update the firmware on Mac. there is no issue. You can follow below instructions. thanks.
<LINK_TEXT text=“http://wiki.seeedstudio.com/ReSpeaker_M … e-firmware”>http://wiki.seeedstudio.com/ReSpeaker_Mic_Array_v2.0/#update-firmware</LINK_TEXT>
Great, thanks for the answer
Incidentally, for other people viewing this thread, pyusb relies on libusb to be installed on your mac to do the low-level dfu communications with your usb devices. See here <LINK_TEXT text=“https://stackoverflow.com/questions/385 … n-mac-os-x”>https://stackoverflow.com/questions/3853634/how-to-set-up-libusb-on-mac-os-x</LINK_TEXT> on how to do that.