Hi
Let me define the connection Jack this way
1-the tip
2-first ring
3-second ring
4-the body or shield
Using a continuity checker seems that 3 and 4 are connected together and to GND (the body of the nearby USB connector)
I connected two speakers in this way: one between 1 and 3 and the other between 2 and 4. They work.
The doubt I have arises from the audio codec data-sheet. This document shows that Speakers shall be connected BTL way, i.e. to positive and negative output of each channel, not to GND.
Where am I wrong?,
There is something (I do not know) between jack pins and speaker outputs of the encoder?
Thanks
Angelo M
hi Angelo~
Please refer to below schematic. Hope it can help.