ReSpeaker Mic Array v2 48KHz support

Good morning,

I am currently working with a ReSpeaker Far-field Mic Array v2 development board and am having problems flashing and testing the original firmware that supports 48 KHz sampling rate.

Although I have written code that works well with every version of the 16KHz compatible firmware files, when I flash the 48KHz ones I can’t even record audio. I have tested using python scripts and audacity.
In the latter case, Audacity can’t even open the device to start recording.

I always flash the firmware using the proper method and on an Ubuntu environment.

Is this an hardware issue (like the XMOS chip not supporting 48KHz) or am I doing something wrong?

Thank you.

Hi @nuno.fernandes
The Max Sample Rate of the ReSpeaker Far-field Mic Array v2 is 16Khz, so this is related to the hardware limit.

Ok! Thank you very much for your help!