Respeaker Mic Array V2.0 (Windows 10 usage)

Hello,

I need to detect audio sources (voice) within certain angle (90-120 degrees) and located closer than 2 meters. The other sounds must be suppressed. I am using Windows 10

  1. Is it possible to setup this device to fulfill this task out of the box without programming?
  2. If not, is it possible program the device (C/С++/С#/etc libraries) to accomplish the task under Windows 10.

Thank you,

I would like to know this too. Does anyone have any idea on how to set the DOAANGLE to within 70 - 110 degrees range? I only need this parameter set and have the audio coming out from USB Audio device

I mean, if i have to write and compile code on XM3000… i would. but i don’t even have a single starting point.