Hello,
I just have some questions about the concerning the ReSpeaker Mic Array V2.0.
- Can the ReSpeaker Mic Array V2.0 output realtime AEC filtered audio from its 3.5mm audio jack? In my application, I’m hoping to use the ReSpeaker as a microphone for an intercom system in a noisey environment. I need the filtered audio to be output to a transceiver for a private voice radio system. Once programmed, this possible without external hardware?
- Is it possible to add a delay to the audio output without external hardware? If, in my application, I need to add a delay of up to 1 second to the recorded audio, is the ReSpeaker Mic Array V2.0 capable of this? Does it have built in memory?
Thank you!