ReSpeaker Lite Voice Assistant Kit Schematic

Hi

Im looking to write firmware for the XMOS chip on the ReSpeaker Lite Voice Assistant Kit
However im not sure what pins are being used to connect the ESP32 to the XMOS XU316.

Please can someone clarity the pins that are connected on both chips? The ESP32 is using
GPIO8 - bclk,
GPIO7 - ws/lrck,
GPIO43 - dout,
GPIO44 - din

But what pins on the XMOS are being used to recieve these signals?

Is there a schematic available for this Kit, or a link to the source code that was modified from the original found here?

Kind regards

Hello Seeed Team,

Coule you please provide the full schematic of Re-Speaker Lite please , not sure why it is not available on the wiki,in spite of being open hardware.

Only the headphone jack detection circuit diagram is here:

Hi,
Did you ever get a link to the full schematic? If so, where can I find it?

The ReSpeaker Lite Voice Assistant Kit integrates an ESP32-S3 microcontroller with an XMOS XU316 DSP chip, utilizing I2S interfaces for audio data exchange. The ESP32-S3 employs the following GPIOs for I2S communication: