Hi PJ,
Asking about the BIN, you probably want to know about that one: ReSpeaker Lite Voice Assistant Kit | Seeed Studio Wiki.
Can you give me a hint on how to blank the S3?
Chip shows in Arduino, but when I try to upload a program, it always ends up with the following:
Sketch uses 235997 bytes (7%) of program storage space. Maximum is 3342336 bytes.
Global variables use 18192 bytes (5%) of dynamic memory, leaving 309488 bytes for local variables. Maximum is 327680 bytes.
esptool.py v4.5.1
Serial port COM5
Connecting......................................
A fatal error occurred: Failed to connect to ESP32-S3: No serial data received.
For troubleshooting steps visit: https://docs.espressif.com/projects/esptool/en/latest/troubleshooting.html
May I ask again, if there should be some visual signal when ESP is in the bootloader mode?
Best!