Hello everyone,
I have purchased the Respeaker core v2 and installed Mycroft successfully tough the Hot Word detection isn’t precise enough for me. After some digging, I’ve seen that Mycroft is using the SIMD processor instruction for their Precise engine.
I have used cat /proc/cpuinfo (see the result below) and it seems like the SIMD instruction isn’t available. Though Rockship RK3229, which the SBC is based on, claim to support this from the Wiki and the datasheet.
Am I missing something? Or the Respeaker Core v2 doesn’t have the instruction?
respeaker@respeaker:~$ cat /proc/cpuinfo
processor : 0
model name : ARMv7 Processor rev 5 (v7l)
BogoMIPS : 24.00
Features : half thumb fastmult vfp edsp thumbee neon vfpv3 tls vfpv4 idiva idivt vfpd32 lpae evtstrm
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x0
CPU part : 0xc07
CPU revision : 5