Hello,
I am using the ReSpeaker Core v2. Can I connect the 4-Mic Linear Array Kit for Raspberry Pi to it?
As far as I see I2C connection is available but I do not have the 40 Pin raspberry header.
Further I need to exchange the FFC cable, 20cm are not enough for my application. Is there a MAX length? I could not find these information…
Thank You,
Miguel
Hi Miguel
The respeaker core v2.0 integrates the mics. why do you plan to attach the mic pi hat?
for the FFC cable, here is the datasheet for the cable, you shall be able to find it from internet. thanks.
30Pins, 0.5mm distance
<LINK_TEXT text=“https://www.amazon.com/30-pin-Forward-D … 30+pin+ffc”>https://www.amazon.com/30-pin-Forward-Direction-Ribbon-Cable/dp/B00W8W9YYG/ref=sr_1_2?ie=UTF8&qid=1541153178&sr=8-2&keywords=30+pin+ffc</LINK_TEXT>