Respeaker Core V1.0 total factory reset, how do I do it?

Thanks for your reply, I tried a few commands here are the results :
root@ReSpeaker:/# mount
rootfs on / type rootfs (rw)
/dev/root on /rom type squashfs (ro,relatime)
proc on /proc type proc (rw,nosuid,nodev,noexec,noatime)
sysfs on /sys type sysfs (rw,nosuid,nodev,noexec,noatime)
tmpfs on /tmp type tmpfs (rw,nosuid,nodev,noatime)
overlayfs:/overlay on / type overlay (rw,noatime,lowerdir=/,upperdir=/overlay/upper,workdir=/overlay/work)
tmpfs on /dev type tmpfs (rw,nosuid,relatime,size=512k,mode=755)
devpts on /dev/pts type devpts (rw,nosuid,noexec,relatime,mode=600)
debugfs on /sys/kernel/debug type debugfs (rw,noatime)
mountd(pid1620) on /tmp/run/mountd type autofs (rw,relatime,fd=5,pgrp=1618,timeout=60,minproto=5,maxproto=5,indirect)
/dev/mmcblk0p1 on /tmp/run/mountd/mmcblk0p1 type vfat (rw,relatime,uid=1000,gid=1000,fmask=0022,dmask=0022,codepage=437,iocharset=iso8859-1,shortname=mixed,errors=remount-ro)

root@ReSpeaker:/# cat /etc/os-release
cat: can’t open ‘/etc/os-release’: No such file or directory

root@ReSpeaker:/# umount /overlay
umount: can’t umount /overlay: Invalid argument

root@ReSpeaker:/#

No mention of Debian or Raspbian.

Could you expand a little bit on the reflashing please? I have tried to flash with Balena etcher using the “Ramips Openwrt latest LinkIt7688 Squashfs…” file but Balena says there is no partition table, “might not be recognised or bootable” etc. Do I just carry on anyway or does that mean it won’t work ?

Or did you mean something else entirely ?