Hi!
I can’t connect my smartphone and laptop to Respeaker Core V.2 in slave-mode (play music on board).
I’m using <LINK_TEXT text=“http://wiki.seeedstudio.com/ReSpeaker_C … reparation”>http://wiki.seeedstudio.com/ReSpeaker_Core_v2.0/#preparation</LINK_TEXT> guide to run bluetooth.
My kernel version:
</s>Linux v2 4.4.138-respeaker-r0 #2 SMP Wed Jul 25 11:29:18 CST 2018 armv7l GNU/Linux<e>
There is no additional packages, clean “respeaker-debian-9-lxqt-flasher-20180801-4gb.img.xz” image (I checked sha256 sum, it’s correct)
[code]
respeaker@v2:~$ ps aux | grep bt | grep -v grep
root       573  3.3  1.2  28548 12208 ?        Ssl  15:52   0:17 /usr/bin/python3 /usr/bin/bt-auto-connect.py
ps aux | grep blue | grep -v grep
root       579  0.0  0.2   3956  2220 ?        Ss   15:52   0:00 /bin/bash /usr/bin/re-bluetooth
root       693  0.9  0.4   7828  4148 ?        Ss   15:52   0:04 /usr/lib/bluetooth/bluetoothd
ps aux | grep brcm | grep -v grep
root       782  0.0  0.0   1228   300 ?        S    15:52   0:00 brcm_patchram_plus --enable_hci --no2bytes --use_baudrate_for_download --tosleep 200000 --baudrate 1500000 --patchram /system/etc/firmware/bcm43438a0.hcd /dev/ttyS1
systemctl | grep ReSpeaker
brcm.service                                                                                  loaded activating start     start ReSpeaker Bt brcm service
bt-auto-connect.service                                                                       loaded active     running         ReSpeaker bluetooth auto connect service
[/code]
My laptop - MacBook Air 2015. I see device, can pair it, but after 5-10 seconds after connect it drops
My smartphone - Xioami A1. I can’t see device, but I can see my phone from Respeaker using bluetoothctl.