I’m looking through hardware options for voice control using snips in conjunction with Homeassistant.
I see a number of setup using one of the Respeaker Mic arrays attached to Raspberry pi, which looks like a decent option. What do you use for Raspberry pi cases for something like this to keep everything contained?
The other thing I’ve seen is the Respeaker core 2.0. Which is a self contained board with the Mic array already on board.
Hi,
If you use ReSpeaker with Raspberry pi you can utilize the Raspberry Pi community resources and you can also use it for another purpose, and if you want to standalone device go for the ReSpeaker Core 2.0 .