I’m looking through hardware options for voice control using snips in conjunction with Homeassistant.
I see a number of setup using one of the Respeaker Mic arrays attached to Raspberry pi, which looks like a decent option. What do you use for Raspberry pi cases for something like this to keep everything contained?
The other thing I’ve seen is the Respeaker core 2.0. Which is a self contained board with the Mic array already on board. It looks like it would fit neatly in a case Respeaker sells and be a nice self-contained unit. It looks like according to it is supported by snips, and the price would be close to a new Pi + case + mic array anyway. Has anyone used one of these before?
thanks
reverse phone lookup nba reddit pcpartpicker
Hi,
For option One you can use a 3d printed case to enclose everything. and for the second option Respeaker core 2.0 also good choice, if you don’t want to use raspberry Pi.