ReSpeaker 6-Mic Array and Raspberry 5 compatibility?

While there may not be official documentation confirming compatibility between the ReSpeaker 6-Mic Array and the Raspberry Pi 5, the ReSpeaker series has historically worked well with previous versions of Raspberry Pi (like the Pi 4). Given that the Raspberry Pi 5 features improved hardware but retains similar GPIO pin setups, it’s highly likely that the 6-Mic Array will function correctly.

However, since the Raspberry Pi 5 is newer, certain drivers or firmware updates may be required for optimal performance. Checking Seeed Studio’s forums or community pages may provide additional insights from users who have tested this configuration.

1 Like