I am following the instructions here to set up with my Jetson Nano.
Drivera are installed OK and I can speak into the mics and hear the output back (in one ear only) in my headphones. So I wanted to run all the other tools.
Did you miss the part where i said i got the drivers installed on the Jetson Nano? I did that by following the Jetson Nano section. But now I have that installed i want to go ahead and do something useful with it which is why I wanted to install all the components for the alsamixer, LEDs, button etc. Are you saying I can use that without having to perform the installation of modules shown in the Raspberry Pi section?