Hi,
I have a Respeaker 2-Mics Pi Hat. It have two grove connectors that are I2C and GPIO12.
I bought two sensors with Grove I2C (Grove - Laser PM2.5 Air Quality Sensor for Arduino - HM3301, Grove - CO2 & Temperature & Humidity Sensor for Arduino - SCD30). Both sensors are I2C.
I would like to connect these sensors to Respeaker 2-Mics Pi Hat.
Is that possible?
Thank you. I’ll try both ways. I gonna write a result later.
I tested with other I2C sensor .(Grove I2C High Acuuracy Temp&Humi Sensor(SHT35))
1st way is very easy and it works!
2nd way does not work.
I tried followings:
[code]
# set i2c on
sudo raspi-config nonint do_i2c 0
respeaker 2mic uses gpio12,13 for Grove GPIO
echo “dtoverlay=i2c5” | sudo tee -a /boot/config.txt
sudo reboot
set gpio12,13 alt5 and pull up
sudo raspi-gpio set 12-13 a5 pu
check i2c-5 but no address appears
i2cdetect -y 5
[/code]
Which one is worked and which one is not worked?
Sorry for confusing.
Connecting Grove I2C Sensor using Grove-I2C Hub to Grove I2C port is worked (1st way).
Connecting Grove I2C sensor directly to Grove GPIO port and setting configuration is not worked (2nd way).
I tested on Raspberry PI 4B with ReSpeaker 2-Mics Pi Hat.
Hi,
Thanks for the replay,
may I now the settings configuration.