Respeaker 2 hat

Hello

I have respeaker 2 hat connected to raspberry pi zero. Everything work perfect, however I want to connect l2c device (led 8x16 i2c supported) to respeaker i2c port.

When I check i2c port, it looks like being used by sound driver, that’s why I cannot use it.

Is there a way to configure i2c to use external device (not grove i2c) ?

Regards

Mr. G

the IIC port is a communications bus… so multiple slave devices can communicate… the communication is handled by the master