Hi all,
I recently got a reServer i3 1125G4. I plan on using it as a NAS, and saw from other posts that the included 60W PSU is probably insufficient. I’ve found higher wattage supplies, but I was wondering about the internal power connector.
Is it possible to power the reServer from the “Wafer 2.0mm 8pin” header? See the hardware overview below near the upper right:
If so, is it an 8-Pin EPS +12V connection? I can’t include another image, but its as follows:
Gnd Gnd Gnd Gnd
12V 12V 12V 12V
with the tab at the bottom.
Thanks in advance for any help!