reServer Industrial J4012 Flash Error

Error when flashing Reserver Industrial J4012. Boots into recovery mode without issue, visible in USB list on host Ubunutu with lsusb

Following this guide: reServer Industrial Getting Started | Seeed Studio Wiki

Eventually fails with these errors:

Failed to write to APP
Error flashing external drive
Flash failure
Cleaning up…

Here is the entire log below the line. I removed some lines to fit in the post limit:

hsuser@hsuser-ubuntu:/media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial$ sudo ./tools/kernel_flash/l4t_initrd_flash.sh --flash-only --massflash 1 --network usb0 --showlogs
[sudo] password for hsuser:
/media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial/tools/kernel_flash/l4t_initrd_flash_internal.sh --network usb0 --usb-instance 1-5 --device-instance 0 --flash-only --external-device nvme0n1p1 -c “tools/kernel_flash/flash_l4t_nvme.xml” -S 80GiB --network usb0 reserver-orin-industrial external


  •                                        *
    
  • Step 1: Build the flashing environment *
  •                                        *
    

Create flash environment 0
/media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial/bootloader /media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial
/media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial
Finish creating flash environment 0.


  •                                              *
    
  • Step 2: Boot the device with flash initrd image *
  •                                              *
    

/media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial/temp_initrdflash/bootloader0 /media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial
./tegraflash.py --bl uefi_jetson_with_dtb_sigheader.bin.encrypt --bct br_bct_BR.bct --securedev --bldtb tegra234-p3767-0000-p3509-a02.dtb --applet rcm_2_encrypt.rcm --applet_softfuse rcm_1_encrypt.rcm --cmd “rcmboot” --cfg secureflash.xml --chip 0x23 --mb1_bct mb1_bct_MB1_sigheader.bct.encrypt --mem_bct mem_rcm_sigheader.bct.encrypt --mb1_cold_boot_bct mb1_cold_boot_bct_MB1_sigheader.bct.encrypt --mb1_bin mb1_t234_prod_aligned_sigheader.bin.encrypt --psc_bl1_bin psc_bl1_t234_prod_aligned_sigheader.bin.encrypt --mem_bct_cold_boot mem_coldboot_sigheader.bct.encrypt --bins “psc_fw pscfw_t234_prod_sigheader.bin.encrypt; mts_mce mce_flash_o10_cr_prod_sigheader.bin.encrypt; mb2_applet applet_t234_sigheader.bin.encrypt; mb2_bootloader mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt; xusb_fw xusb_t234_prod_sigheader.bin.encrypt; dce_fw display-t234-dce_sigheader.bin.encrypt; nvdec nvdec_t234_prod_sigheader.fw.encrypt; bpmp_fw bpmp_t234-TE990M-A1_prod_sigheader.bin.encrypt; bpmp_fw_dtb tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt; sce_fw camera-rtcpu-sce_sigheader.img.encrypt; rce_fw camera-rtcpu-t234-rce_sigheader.img.encrypt; ape_fw adsp-fw_sigheader.bin.encrypt; spe_fw spe_t234_sigheader.bin.encrypt; tos tos-optee_t234_sigheader.img.encrypt; eks eks_t234_sigheader.img.encrypt; kernel boot0.img; kernel_dtb tegra234-p3767-0000-p3509-a02.dtb” --secondary_gpt_backup --bct_backup --boot_chain A --instance 1-5
Welcome to Tegra Flash
version 1.0.0
Type ? or help for help and q or quit to exit
Use ! to execute system commands

Entering RCM boot

[ 0.0508 ] mb1_t234_prod_aligned_sigheader.bin.encrypt filename is from --mb1_bin
[ 0.0508 ] psc_bl1_t234_prod_aligned_sigheader.bin.encrypt filename is from --psc_bl1_bin
[ 0.0508 ] rcm boot with presigned binaries
[ 0.0522 ] tegrarcm_v2 --instance 1-5 --new_session --chip 0x23 0 --uid --download bct_br br_bct_BR.bct --download mb1 mb1_t234_prod_aligned_sigheader.bin.encrypt --download psc_bl1 psc_bl1_t234_prod_aligned_sigheader.bin.encrypt --download bct_mb1 mb1_bct_MB1_sigheader.bct.encrypt
[ 0.0535 ] BR_CID: 0x80012344705DD80B1400000006038140
[ 0.0672 ] Sending bct_br
[ 0.0825 ] Sending mb1
[ 0.0831 ] Sending psc_bl1
[ 0.0946 ] Sending bct_mb1
[ 0.1011 ] Generating blob for T23x
[ 0.1098 ] tegrahost_v2 --chip 0x23 0 --generateblob blob.xml blob.bin
[ 0.1134 ] The number of images in blob is 18
[ 0.1155 ] blobsize is 73509987
[ 0.1164 ] Added binary blob_uefi_jetson_with_dtb_sigheader.bin.encrypt of size 3190848
[ 0.1791 ] Added binary blob_pscfw_t234_prod_sigheader.bin.encrypt of size 375168
[ 0.1801 ] Added binary blob_mce_flash_o10_cr_prod_sigheader.bin.encrypt of size 190592
[ 0.1811 ] Added binary blob_applet_t234_sigheader.bin.encrypt of size 277312
[ 0.1819 ] Not supported type: mb2_applet
[ 0.1824 ] Added binary blob_mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt of size 437984
[ 0.1835 ] Added binary blob_xusb_t234_prod_sigheader.bin.encrypt of size 164864
[ 0.1844 ] Added binary blob_display-t234-dce_sigheader.bin.encrypt of size 9097216
[ 0.1889 ] Added binary blob_nvdec_t234_prod_sigheader.fw.encrypt of size 294912
[ 0.1915 ] Added binary blob_bpmp_t234-TE990M-A1_prod_sigheader.bin.encrypt of size 1048000
[ 0.1930 ] Added binary blob_tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt of size 138880
[ 0.1946 ] Added binary blob_camera-rtcpu-sce_sigheader.img.encrypt of size 166304
[ 0.1952 ] Added binary blob_camera-rtcpu-t234-rce_sigheader.img.encrypt of size 537952
[ 0.1960 ] Added binary blob_adsp-fw_sigheader.bin.encrypt of size 400960
[ 0.1968 ] Added binary blob_spe_t234_sigheader.bin.encrypt of size 270336
[ 0.1977 ] Added binary blob_tos-optee_t234_sigheader.img.encrypt of size 1064752
[ 0.1985 ] Added binary blob_eks_t234_sigheader.img.encrypt of size 9232
[ 0.1994 ] Added binary blob_boot0.img of size 55498752
[ 0.2470 ] Added binary blob_tegra234-p3767-0000-p3509-a02.dtb of size 344819
[ 0.3163 ] tegrarcm_v2 --instance 1-5 --chip 0x23 0 --pollbl --download bct_mem mem_rcm_sigheader.bct.encrypt --download blob blob.bin
[ 0.3175 ] BL: version 0.32.0.1-t234-54845784-1cb23efd last_boot_error: 0
[ 0.3324 ] Sending bct_mem
[ 0.3449 ] Sending blob
[ 3.5066 ] RCM-boot started

/media/hsuser/Backup/mfi_reserver-orin-nx-16g-industrial-5.1-35.3.1-2023-08-05/mfi_reserver-orin-industrial


  •                                 *
    
  • Step 3: Start the flashing process *
  •                                 *
    

Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for target to boot-up…
Waiting for device to expose ssh …RTNETLINK answers: File exists
RTNETLINK answers: File exists
Waiting for device to expose ssh …Run command: flash on fc00:1:1:0::2
SSH ready
blockdev: cannot open /dev/mmcblk0boot0: No such file or directory
[ 0]: l4t_flash_from_kernel: Starting to create gpt for emmc
Active index file is /mnt/internal/flash.idx
Number of lines is 58
max_index=57
[ 2]: l4t_flash_from_kernel: Successfully create gpt for emmc
[ 2]: l4t_flash_from_kernel: Starting to create gpt for external device
Active index file is /mnt/external/flash.idx
Number of lines is 18
max_index=17
writing item=1, 9:0:primary_gpt, 512, 19968, gpt_primary_9_0.bin, 16896, fixed--0, 1d1515da6c9b4d250b3dd33e601c604a0807dac2
Writing primary_gpt partition with gpt_primary_9_0.bin
Offset is not aligned to K Bytes, no optimization is applied
dd if=/mnt/external/gpt_primary_9_0.bin of=/dev/nvme0n1 bs=1 skip=0 seek=512 count=16896
16896+0 records in
16896+0 records out
16896 bytes (17 kB, 16 KiB) copied, 0.0228882 s, 738 kB/s
Writing primary_gpt partition done
Error: The backup GPT table is corrupt, but the primary appears OK, so that will be used.
Warning: Not all of the space available to /dev/nvme0n1 appears to be used, you can fix the GPT to use all of the space (an extra 50069679 blocks) or continue with the current setting?
Writing secondary_gpt partition with gpt_secondary_9_0.bin
Offset is not aligned to K Bytes, no optimization is applied
dd if=/mnt/external/gpt_secondary_9_0.bin of=/dev/nvme0n1 bs=1 skip=0 seek=102399983104 count=16896
16896+0 records in
16896+0 records out
16896 bytes (17 kB, 16 KiB) copied, 0.0209206 s, 808 kB/s
Writing secondary_gpt partition done
Fix/Ignore? Fix
Fix/Ignore? Fix
Error: The backup GPT table is not at the end of the disk, as it should be. Fix, by moving the backup to the end (and removing the old backup)?
Warning: Not all of the space available to /dev/nvme0n1 appears to be used, you can fix the GPT to use all of the space (an extra 50069679 blocks) or continue with the current setting?
Model: NHESR128GTLEW-I3C-2 (nvme)
Disk /dev/nvme0n1: 128GB
Sector size (logical/physical): 512B/512B
Partition Table: gpt
Disk Flags:

Number Start End Size File system Name Flags
1 20.5kB 85.9GB 85.9GB ext4 APP msftdata
2 85.9GB 86.0GB 67.1MB kernel msftdata
3 86.0GB 86.0GB 459kB kernel-dtb msftdata
4 86.0GB 86.0GB 33.6MB reserved_for_chain_A_user msftdata
5 86.0GB 86.1GB 67.1MB kernel_b msftdata
6 86.1GB 86.1GB 459kB kernel-dtb_b msftdata
7 86.1GB 86.1GB 33.6MB reserved_for_chain_B_user msftdata
8 86.1GB 86.2GB 83.9MB recovery msftdata
9 86.2GB 86.2GB 524kB recovery-dtb msftdata
10 86.2GB 86.5GB 315MB RECROOTFS msftdata
11 86.5GB 86.6GB 67.1MB fat32 esp boot, esp
12 86.6GB 86.7GB 83.9MB recovery_alt msftdata
13 86.7GB 86.7GB 524kB recovery-dtb_alt msftdata
14 86.7GB 86.7GB 67.1MB esp_alt msftdata
15 86.7GB 102GB 15.7GB UDA msftdata

[ 16]: l4t_flash_from_kernel: Expanding last partition to fill the storage device
[ 16]: l4t_flash_from_kernel: Successfully create gpt for external device
[ 16]: l4t_flash_from_kernel: Starting to flash to emmc
[ 16]: l4t_flash_from_kernel: Starting to flash to external device
Active index file is /mnt/internal/flash.idx
Active index file is /mnt/external/flash.idx
Flash index file is /mnt/internal/flash.idx
Number of lines is 58
max_index=57
Number of lines is 18
max_index=17
Number of lines is 58
max_index=57
[ 16]: l4t_flash_from_kernel: Starting to flash to qspi
writing item=0, 9:0:master_boot_record, 0, 512, mbr_9_0.bin, 512, fixed--0, 694898d1c345bdb31b377790ed7fc0b0db184bf7
QSPI storage size: 67108864 bytes.
writing item=1, 9:0:primary_gpt, 512, 19968, gpt_primary_9_0.bin, 16896, fixed--0, 1d1515da6c9b4d250b3dd33e601c604a0807dac2
writing item=2, 9:0:APP, 20480, 85899345920, , , fixed--1,
Formatting APP partition /dev/nvme0n1p1 …
mke2fs 1.45.5 (07-Jan-2020)
Discarding device blocks: done
Creating filesystem with 20971520 4k blocks and 5242880 inodes
Filesystem UUID: 58b0ae38-6e5e-4e1d-8fa2-409149ed3eaf
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208,
4096000, 7962624, 11239424, 20480000

Allocating group tables: done
Writing inode tables: done
Creating journal (131072 blocks): [ 17]: l4t_flash_from_kernel: Successfully flash the emmc
done
Writing superblocks and filesystem accounting information: done

Formatting APP parition done
mount: only root can do that (effective UID is 1000)
[ 18]: l4t_flash_from_kernel: Failed to mount APP partition /dev/nvme0n1p1
Erased 67108864 bytes from address 0x00000000 in flash
Flash index file is /mnt/internal/flash.idx
Number of lines is 58
max_index=57
Writing br_bct_BR.bct (parittion: BCT) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/br_bct_BR.bct
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:0
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00000000 in flash
[ 179]: l4t_flash_from_kernel: QSPI erase block size is 65536
[ 179]: l4t_flash_from_kernel: Writing 16 copies of /mnt/internal/br_bct_BR.bct
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:65536
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00010000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:131072
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00020000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:196608
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00030000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:262144
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00040000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:327680
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00050000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:393216
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00060000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:458752
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00070000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:524288
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00080000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:589824
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x00090000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:655360
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x000a0000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:720896
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x000b0000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:786432
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x000c0000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:851968
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x000d0000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:917504
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x000e0000 in flash
Writing /mnt/internal/br_bct_BR.bct (8192 bytes) into /dev/mtd0:983040
Copied 8192 bytes from /mnt/internal/br_bct_BR.bct to address 0x000f0000 in flash
Writing mb1_t234_prod_aligned_sigheader.bin.encrypt (parittion: A_mb1) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/mb1_t234_prod_aligned_sigheader.bin.encrypt
Writing /mnt/internal/mb1_t234_prod_aligned_sigheader.bin.encrypt (268336 bytes) into /dev/mtd0:1048576
Copied 268336 bytes from /mnt/internal/mb1_t234_prod_aligned_sigheader.bin.encrypt to address 0x00100000 in flash
Writing psc_bl1_t234_prod_aligned_sigheader.bin.encrypt (parittion: A_psc_bl1) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/psc_bl1_t234_prod_aligned_sigheader.bin.encrypt
Writing /mnt/internal/psc_bl1_t234_prod_aligned_sigheader.bin.encrypt (119616 bytes) into /dev/mtd0:1572864
Copied 119616 bytes from /mnt/internal/psc_bl1_t234_prod_aligned_sigheader.bin.encrypt to address 0x00180000 in flash
Writing mb1_cold_boot_bct_MB1_sigheader.bct.encrypt (parittion: A_MB1_BCT) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/mb1_cold_boot_bct_MB1_sigheader.bct.encrypt
Writing /mnt/internal/mb1_cold_boot_bct_MB1_sigheader.bct.encrypt (17056 bytes) into /dev/mtd0:1835008
Copied 17056 bytes from /mnt/internal/mb1_cold_boot_bct_MB1_sigheader.bct.encrypt to address 0x001c0000 in flash
Writing mem_coldboot_sigheader.bct.encrypt (parittion: A_MEM_BCT) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/mem_coldboot_sigheader.bct.encrypt
Writing /mnt/internal/mem_coldboot_sigheader.bct.encrypt (243712 bytes) into /dev/mtd0:1966080
Copied 243712 bytes from /mnt/internal/mem_coldboot_sigheader.bct.encrypt to address 0x001e0000 in flash
[ 180]: l4t_flash_from_kernel: Warning: skip writing A_tsec-fw partition as no image is specified
Writing nvdec_t234_prod_sigheader.fw.encrypt (parittion: A_nvdec) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/nvdec_t234_prod_sigheader.fw.encrypt
Writing /mnt/internal/nvdec_t234_prod_sigheader.fw.encrypt (294912 bytes) into /dev/mtd0:3276800
Copied 294912 bytes from /mnt/internal/nvdec_t234_prod_sigheader.fw.encrypt to address 0x00320000 in flash
Writing mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt (parittion: A_mb2) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt
Writing /mnt/internal/mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt (437984 bytes) into /dev/mtd0:4325376
Copied 437984 bytes from /mnt/internal/mb2_t234_with_mb2_cold_boot_bct_MB2_sigheader.bin.encrypt to address 0x00420000 in flash
Writing xusb_t234_prod_sigheader.bin.encrypt (parittion: A_xusb-fw) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/xusb_t234_prod_sigheader.bin.encrypt
Writing /mnt/internal/xusb_t234_prod_sigheader.bin.encrypt (164864 bytes) into /dev/mtd0:4849664
Copied 164864 bytes from /mnt/internal/xusb_t234_prod_sigheader.bin.encrypt to address 0x004a0000 in flash
Writing bpmp_t234-TE990M-A1_prod_sigheader.bin.encrypt (parittion: A_bpmp-fw) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/bpmp_t234-TE990M-A1_prod_sigheader.bin.encrypt
Writing /mnt/internal/bpmp_t234-TE990M-A1_prod_sigheader.bin.encrypt (1048000 bytes) into /dev/mtd0:5111808
Copied 1048000 bytes from /mnt/internal/bpmp_t234-TE990M-A1_prod_sigheader.bin.encrypt to address 0x004e0000 in flash
Writing tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt (parittion: A_bpmp-fw-dtb) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt
Writing /mnt/internal/tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt (138880 bytes) into /dev/mtd0:6684672
Copied 138880 bytes from /mnt/internal/tegra234-bpmp-3767-0000-a02-3509-a02_with_odm_sigheader.dtb.encrypt to address 0x00660000 in flash
Writing pscfw_t234_prod_sigheader.bin.encrypt (parittion: A_psc-fw) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/pscfw_t234_prod_sigheader.bin.encrypt
Writing /mnt/internal/pscfw_t234_prod_sigheader.bin.encrypt (375168 bytes) into /dev/mtd0:10878976
Copied 375168 bytes from /mnt/internal/pscfw_t234_prod_sigheader.bin.encrypt to address 0x00a60000 in flash
Writing mce_flash_o10_cr_prod_sigheader.bin.encrypt (parittion: A_mts-mce) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/mce_flash_o10_cr_prod_sigheader.bin.encrypt
Writing /mnt/internal/mce_flash_o10_cr_prod_sigheader.bin.encrypt (190592 bytes) into /dev/mtd0:11665408
Copied 190592 bytes from /mnt/internal/mce_flash_o10_cr_prod_sigheader.bin.encrypt to address 0x00b20000 in flash
Writing sc7_t234_prod_sigheader.bin.encrypt (parittion: A_sc7) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/sc7_t234_prod_sigheader.bin.encrypt
Writing /mnt/internal/sc7_t234_prod_sigheader.bin.encrypt (167376 bytes) into /dev/mtd0:12189696
Copied 167376 bytes from /mnt/internal/sc7_t234_prod_sigheader.bin.encrypt to address 0x00ba0000 in flash
Writing camera-rtcpu-t234-rce_sigheader.img.encrypt (parittion: B_rce-fw) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/camera-rtcpu-t234-rce_sigheader.img.encrypt
Writing /mnt/internal/camera-rtcpu-t234-rce_sigheader.img.encrypt (537952 bytes) into /dev/mtd0:61014016
Copied 537952 bytes from /mnt/internal/camera-rtcpu-t234-rce_sigheader.img.encrypt to address 0x03a30000 in flash
Writing adsp-fw_sigheader.bin.encrypt (parittion: B_adsp-fw) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/adsp-fw_sigheader.bin.encrypt
Writing /mnt/internal/adsp-fw_sigheader.bin.encrypt (400960 bytes) into /dev/mtd0:62062592
Copied 400960 bytes from /mnt/internal/adsp-fw_sigheader.bin.encrypt to address 0x03b30000 in flash
[ 215]: l4t_flash_from_kernel: Warning: skip writing B_reserved_on_boot partition as no image is specified
[ 215]: l4t_flash_from_kernel: Warning: skip writing uefi_variables partition as no image is specified
[ 215]: l4t_flash_from_kernel: Warning: skip writing uefi_ftw partition as no image is specified
[ 215]: l4t_flash_from_kernel: Warning: skip writing worm partition as no image is specified
Writing bct_backup.img (parittion: BCT-boot-chain_backup) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/bct_backup.img
Writing /mnt/internal/bct_backup.img (32768 bytes) into /dev/mtd0:66715648
Copied 32768 bytes from /mnt/internal/bct_backup.img to address 0x03fa0000 in flash
[ 215]: l4t_flash_from_kernel: Warning: skip writing reserved_partition partition as no image is specified
Writing gpt_secondary_3_0.bin (parittion: secondary_gpt_backup) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/gpt_secondary_3_0.bin
Writing /mnt/internal/gpt_secondary_3_0.bin (16896 bytes) into /dev/mtd0:66846720
Copied 16896 bytes from /mnt/internal/gpt_secondary_3_0.bin to address 0x03fc0000 in flash
Writing qspi_bootblob_ver.txt (parittion: B_VER) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/qspi_bootblob_ver.txt
Writing /mnt/internal/qspi_bootblob_ver.txt (109 bytes) into /dev/mtd0:66912256
Copied 109 bytes from /mnt/internal/qspi_bootblob_ver.txt to address 0x03fd0000 in flash
Writing qspi_bootblob_ver.txt (parittion: A_VER) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/qspi_bootblob_ver.txt
Writing /mnt/internal/qspi_bootblob_ver.txt (109 bytes) into /dev/mtd0:66977792
Copied 109 bytes from /mnt/internal/qspi_bootblob_ver.txt to address 0x03fe0000 in flash
Writing gpt_secondary_3_0.bin (parittion: secondary_gpt) into /dev/mtd0
Sha1 checksum matched for /mnt/internal/gpt_secondary_3_0.bin
Writing /mnt/internal/gpt_secondary_3_0.bin (16896 bytes) into /dev/mtd0:67091968
Copied 16896 bytes from /mnt/internal/gpt_secondary_3_0.bin to address 0x03ffbe00 in flash
[ 216]: l4t_flash_from_kernel: Successfully flash the qspi
[ 216]: l4t_flash_from_kernel: The device size indicated in the partition layout xml is smaller than the actual size. This utility will try to fix the GPT.
[ 216]: l4t_flash_from_kernel: Failed to write to APP
[ 216]: l4t_flash_from_kernel: Error flashing external device
Flash failure
Cleaning up…

Update: Tried Method 2 and it flashed successfully.

Not sure if related but might help someone in the future.

I got the exact same error when i forgot to unplug a contour USB receiver from the device (seeed studio J4012) and tried to flash it.

Unplugged the receiver, jumped the pins, flashed fine after that.

Use a tool like gdisk or parted on Ubuntu to correct the GPT table. You can try the following:

sudo gdisk /dev/nvme0n1

Then, enter the command r to repair the GPT structure, followed by w to write the changes. Alternatively, using parted to check and correct alignment issues might help:

sudo parted /dev/nvme0n1 align-check optimal 1

I keep having this issue recently with different target and host devices which have been flashing without problems previously. What is the cause of this issue? Flashing the target devices using Nvidias SDK manager works. Switching to method 2 throws an error on the host device stating that the image couldn’t be build.

Could you please provide us with detailed information so that we can give you accurate suggestions?