Replacement jst connectors to fit lipo rider pro

Hi,

Just wondering where I can source some connectors to fit the lipo rider pro as the plugs on both panels and lipo batteries don’t fit. Does seeedstudio.com/depot/jst-2- … th=156_158 fit?

Any idea when the lipo rider pro is going to ship with the right plugs on it?

Thanks,

Dave

Yes, you can use the JST connector here:http://www.seeedstudio.com/depot/jst-2-pin-power-connector-p-649.html?cPath=156_158.
The image for this product is not right though. But we will mail the 2.0mm JST connector which fits lipo rider pro.