Relay module Terminal connections

Thanks, I understand how the relay will function once the arduino goes high. Here is the connections I was going to use when I wire the project together. Please let me know if this looks right. Don’t to make a mistake on this. I am working off the drawing in prior post of the relay. Once I get all this worked out I will work out the SKETCH for the Arduino to test it all. My plan is to complete an instructable on the whole process so others will be able to hook all this up in short order and save a lot of time in working out how this could be wired up. I will post the instructable url once I get done with it. I need to get this working for my pumps and valves on my aquaponic units.

ARDUINO to RELAY:

PIN 7 (signal) to Connector 2 center position (COMM-SIGNAL)

5v (RED) or (+) to Connector 2 left of center position (V[size=85]DD[/size] )

GND (BLACK) or (-) to Connector 2 right of center position

POWER CORD to RELAY to OUTLET CONNECTION:

BLACK WIRE from power cord connected to Connector 3 center position

NC or NO connected to HOT side of outlet (small prong side)

WHITE WIRE from power cord connedted to NETURAL OR COMM side of the outlet
(large prong side of the outlet)

GREEN WIRE connected to GND screw of the outlet