reComputer R1000 password

Just got a new product - reComputer R1000 with a raspberry CM4 module on board. Can not find default password to login.

Of course, one of options is to flash new fresh raspbian image, but this is also doesnt work: usbboot cannot load/read CM4, while it is visible in “lsusb”. Will try to move this CM4 module from reComputer IO board to another 100% working IO Board and then give you all know if that works or not.

EDIT:
Of course I did not find password, but was able to download fresh image using another (short ~150mm) cable.