reComputer J401 - Orin NX - sudo apt upgrade or Package Installation Error (JetPack 6.1)

Hello Seeed Studio community,

I’m using the NVIDIA Orin NX module on my reComputer J401. I’ve installed JetPack 6.1 on the device. After the Linux installation, when I try to run the sudo apt upgrade command, or when I attempt to install any package (e.g., sudo apt install keyboard-configuration), I encounter the following error, and the process cannot be completed. This prevents me from updating my system and installing new software.

Error Code:

`Reading package lists… Done
Building dependency tree… Done
Reading state information… Done
keyboard-configuration is already the newest version (1.205ubuntu3).
0 upgraded, 0 newly installed, 0 to remove and 0 not upgraded.
7 not fully installed or removed.
After this operation, 0 B of additional disk space will be used.
Do you want to continue? [Y/n] y
Setting up nvidia-l4t-kernel (5.15.148-tegra-36.4.3-20250107174145) …
Using the existing boot entry ‘primary’
Warning: Cannot get compatible board name.
3767-000-0000–1–recomputer-orin-j401-
TNSPEC 3767-300-0000-N.1-1-0-recomputer-orin-j401-
COMPATIBLE_SPEC 3767-000-0000–1–recomputer-orin-j401-
TEGRA_BOOT_STORAGE nvme0n1
TEGRA_CHIPID 0x23
TEGRA_OTA_BOOT_DEVICE /dev/mtdblock0
TEGRA_OTA_GPT_DEVICE /dev/mtdblock0
Info: Write TegraPlatformCompatSpec with 3767-000-0000–1–recomputer-orin-j401-.
Info: The esp is already mounted to /boot/efi.
Starting kernel post-install procedure.
Rootfs AB is not enabled.
ERROR. Procedure for A_kernel update FAILED.
Cannot install package. Exiting…
dpkg: error processing package nvidia-l4t-kernel (–configure):
installed nvidia-l4t-kernel package post-installation script subprocess returned error exit status 1
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-headers:
nvidia-l4t-kernel-headers depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.3-20250107174145); however:
Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-kernel-headers (–configure):
dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-jetson-io:
nvidia-l4t-jetson-io depends on nvidia-l4t-kernel (>> 5.15.148-tegra-36.4-0); however:
Package nvidia-l4t-kernel is not configured yet.
nvidia-l4t-jetson-io depends on nvidia-l4t-kernel (<< 5.15.148-tegra-36.5-0); however:
Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-jetson-io (–configure):
dependency problems - leaving unconfigured
No apport report written because the error message indicates its a followup error from a previous failure.
No apport report written because the error message indicates its a followup error from a previous
failure.
No apport report written because MaxReports is reached already
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-oot-modules:
nvidia-l4t-kernel-oot-modules depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.3-20250107174145); however:
Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-kernel-oot-modules (–configure):
dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-display-kernel:
nvidia-l4t-display-kernel depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.3-20250107174145); however:
Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-display-kernel (–configure):
dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-oot-headers:
nvidia-l4t-kernel-oot-headers depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.3-20250107174145); however:
Package nvidia-l4t-kernel is not configured yet.

dNo apport report written because MaxReports is reached already
No apport report written because MaxReports is reached already
No apport report written because MaxReports is reached already
pkg: error proces
sing package nvidia-l4t-kernel-oot-headers (–configure):
dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-dtbs:
nvidia-l4t-kernel-dtbs depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.3-20250107174145); however:
Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-kernel-dtbs (–configure):
dependency problems - leaving unconfigured
Processing triggers for nvidia-l4t-initrd (36.4.3-20250107174145) …
Include /etc/nv-update-initrd/list.d/binlist
Include /etc/nv-update-initrd/list.d/modules
nv-update-initrd: Updating /boot/initrd from /etc/nv-update-initrd/list.d for kernel version 5.15.148-tegra…
Add /usr/sbin/nvluks-srv-app
Add /lib/modules/5.15.148-tegra/updates/drivers/net/ethernet/nvidia/nvethernet/nvethernet.ko
Add /lib/modules/5.15.148-tegra/updates/drivers/nvpps/nvpps.ko
Add /lib/modules/5.15.148-tegra/updates/drivers/net/ethernet/realtek/r8126/r8126.ko
Add /lib/modules/5.15.148-tegra/updates/drivers/net/ethernet/realtek/r8168/r8168.ko
Add /lib/modules/5.15.148-tegra/modules*
Add /lib/modules/5.15.148-tegra/kernel/drivers/nvme/host/nvme.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/nvme/host/nvme-core.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/thermal/tegra/tegra-bpmp-thermal.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/pwm/pwm-tegra.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/hwmon/pwm-fan.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/pci/controller/dwc/pcie-tegra194.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/phy/tegra/phy-tegra194-p2u.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/gadget/udc/tegra-xudc.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/typec/ucsi/typec_ucsi.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/typec/ucsi/ucsi_ccg.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/typec/typec.ko
Updating modprobe.d configuration directories for modprobe…
Add config /etc/modprobe.d/alsa-base.conf
Add config /etc/modprobe.d/bcmdhd.conf
Add config /etc/modprobe.d/blacklist-ath_pci.conf
Add config /etc/modprobe.d/blacklist.conf
Add config /etc/modprobe.d/blacklist-firewire.conf
Add config /etc/modprobe.d/blacklist-framebuffer.conf
Add config /etc/modprobe.d/blacklist-modem.conf
Add config-link /etc/modprobe.d/blacklist-oss.conf
Add config /etc/modprobe.d/blacklist-rare-network.conf
Add config /etc/modprobe.d/denylist-nouveau.conf
Add config /etc/modprobe.d/denylist-oot-modules-audio.conf
Add config /etc/modprobe.d/denylist-ramoops.conf
Add config /etc/modprobe.d/denylist-tegra-safety.conf
Add config /etc/modprobe.d/denylist-tpm-ftpm-tee.conf
Add config /etc/modprobe.d/iwlwifi.conf
Add config /etc/modprobe.d/nvgpu.conf
Add config /etc/modprobe.d/nvidia-display.conf
Add config /etc/modprobe.d/tegra-udrm.conf
Add config /lib/modprobe.d/aliases.conf
Add config /lib/modprobe.d/fbdev-blacklist.conf
Add config /lib/modprobe.d/systemd.conf
Cleaning up the temporary directory for updating the initrd…
Errors were encountered while processing:
nvidia-l4t-kernel
nvidia-l4t-kernel-headers
nvidia-l4t-jetson-io
nvidia-l4t-kernel-oot-modules
nvidia-l4t-display-kernel
nvidia-l4t-kernel-oot-headers
nvidia-l4t-kernel-dtbs
E: Sub-process /usr/bin/dpkg returned an error code (1)`

I would greatly appreciate your assistance in resolving this issue.

Thank you