reComputer J401 Carrier Board fails to load VEYE camera /dev/video0 device with Jetpack 6.2

Hi there,

So , You do know the are NOT exact clones. Yes the Device tree and some other items are indeed different than the original. i.e. not 100% plug and play. I would give them some time to test it, now that you brought it to their attention don’t pile on other issues’ or you get no-ware fast. (stick with the compatibility) Once it’s patched correctly it should all work like the others.

HTH
GL :slight_smile: PJ :v: