A new problem with the J401 carrier board and the “Compatibility Issue between reComputer and VEYE Camera”
After flashing Jetpack 6.2 to the J401 Carrier Board with an Orin NX module (reComputer J4011), I applied the USB hub chip firmware fix for the Veye camera (this updates the carrier board USB firmware from FW Version 07F3 to FW Version 08C3):
Solution for the Compatibility Issue between reComputer and VEYE Camera | Seeed Studio Wiki
The Veye camera driver then loads and the camera I2C address is detected:
$ lsmod|grep veye
veyecam 16384 0
tegra_camera 253952 3 nvhost_isp5,veyecam,nvhost_vi5
sudo dmesg|grep veye
[ 7.882004] veyecam 9-003b: probing v4l2 sensor
[ 7.882235] veyecam 9-003b: tegracam sensor driver:veyecam_v2.0.6
[ 7.891278] veyecam 9-003b: camera id is veyecam
[ 7.891970] veyecam 9-003b: sensor is IMX462
[ 7.891973] veyecam 9-003b: board type is ONE board
[ 7.892178] veyecam 9-003b: check hdver 7
[ 7.892372] tegra-camrtc-capture-vi tegra-capture-vi: subdev veyecam 9-003b bound
$ sudo i2cdetect -r -y 9
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: – – – – – – – –
10: – – – – – – – – – – – – – – – –
20: – – – – – – – – – – – – – – – –
30: – – – – – – – – – – – UU – – – –
40: – – – – – – – – – – – – – – – –
50: – – – – – – – – – – – – – – – –
60: – – – – – – – – – – – – – – – –
70: – – – – – – – –
but no device /dev/video* is generated. (It is generated at Jetpack V6.1).
Has anyone else seen this error?
Has anyone successfully enabled the VEYE IMX462 Camera on the J401 carrier board with Jetpack 6.2?
Could there be a solution (updated) for compatibility between reComputer and VEYE Camera at Jetpack 6.2 (it is compatible at Jetpack V6.1).
Thanks
John