ReComputer J1010 reboots on high GPU loads

Hi,
I have a Jetson Nano (production module) mounted on a Seed Studio carrier board J101.

Sometimes when I’m using the GPU on high load, it restarts.

I have found this by storing tegrastats and observing last thing it writes is a 99% frequency on GPU

RAM 3245/3964MB (lfb 107x4MB) SWAP 698/1982MB (cached 38MB) IRAM 0/252kB(lfb 252kB) CPU [11%@1326,35%@1326,13%@1326,11%@1326] EMC_FREQ 18%@1600 GR3D_FREQ 99%@921 VIC_FREQ 9%@192 APE 25 PLL@49C [email protected] PMIC@50C [email protected] AO@64C [email protected] POM_5V_IN 7274/3121 POM_5V_GPU 3570/557 POM_5V_CPU 894/463

I’m using the MAXN mode

sudo jetson_clocks --show

SOC family:tegra210 Machine:NVIDIA Jetson Nano Developer Kit

Online CPUs: 0-3

cpu0: Online=1 Governor=schedutil MinFreq=1200000 MaxFreq=1479000 CurrentFreq=1479000 IdleStates: WFI=1 c7=1

cpu1: Online=1 Governor=schedutil MinFreq=1200000 MaxFreq=1479000 CurrentFreq=1224000 IdleStates: WFI=1 c7=1

cpu2: Online=1 Governor=schedutil MinFreq=1200000 MaxFreq=1479000 CurrentFreq=1479000 IdleStates: WFI=1 c7=1

cpu3: Online=1 Governor=schedutil MinFreq=1200000 MaxFreq=1479000 CurrentFreq=1224000 IdleStates: WFI=1 c7=1

GPU MinFreq=76800000 MaxFreq=921600000 CurrentFreq=76800000

EMC MinFreq=204000000 MaxFreq=1600000000 CurrentFreq=1600000000 FreqOverride=0

Fan: PWM=80

NV Power Mode: MAXN

The power supply is the Raspberry 5 one (up to 27W) so power should not be a problem.

How can I find what is exactly happening? How can I prevent the machine to reboot on high loads?

Thanks