Well, NVdia’s SDK Manager generally doesn’t apply to custom carrier boards, reComputer J3011/J4012 used the J401 carrier board made by us (Industrial version has other carrier boards), and we have made our own jetpacks, refer to the link to flash your device with a physical Ubuntu 20.04/22.04 machine (save strength, waste your time using virtual machine or WSL2…)
-
For reComputer J4012
Flash Jetpack | Seeed Studio Wiki -
For reComputer Industrial J4012
Getting Started with reComputer Industrial | Seeed Studio Wiki -
Follow the guide thoroughly, there might be some versions of jetpacks requires additional operation after you flash/boot your device, that is make a link to your kernel modules and headers (important since many open source drivers required kernel headers to compile), where certain drivers can be loaded. Also, the “sudo apt-get upgrade” command doesn’t apply to custom carrier board either, see Q7- Q9 of Jetson FAQs
-
For USB WiFi adapter, see if your device was supported and additional driver is needed, maybe you’ll need to obtain the driver source and compile the driver yourself.