Wake
1
Hello,
I have flashed my reComputer Industrial J4011 with Jetpack 6.0 and I’m trying to use the DI/DO.
Firstly, the documentation is outdated as Jetpack 6.0 does not have the /sys/class/gpio interface anymore. So instead I used gpioget and gpioset.
Reading the digital inputs works (e. g. gpioget 0 105 for the first digital input).
However, when I connect the digital output, the voltage is always high, doesn’t matter if I set it to 0 or 1 with gpioset.
Is there something else I need to setup? Thank you.
Wake
2
Does no one have the same issue?
Vivio
3
I have J4012, but I have not tested the GPIO yet.
You’ve tried this?
Have you verified the pin configuration and mappings for the digital inputs and outputs on the J4011 board?.